KM Space_Warning_Inserted

KM Space_Warning_Inserted

Address: 22946 (59A2H)
Type: WORD
Access: Read Only
Unit: --
Range: --
Default Value: --
Store Supported: No
Description:

This object contains the state of the internal warnings of the Kollmorgen Space Firmware.

Bit #

Name

Description

Default value

0

Warning_Voltage

1 = Drive voltage is near limit

0 = Ok

0

1

Warning_Temperature

1 = Drive temperature is near limit

0 = Ok

0

2

Warning_EEprom_Near_Write_Overrun

1 = EEprom near Write Overrun.

0 = Ok.

0

3

Warning_EEprom_Near_EOL

1 = EEprom near End of Life

0 = Ok.

0

4

Reserved

Reserved

0

5

Reserved

Reserved

0

6

Reserved

Reserved

0

7

Reserved

Reserved

0

8

Missing_Nominal_Current

1 = Nominal_Current not set and Motor_RL_Detection enabled

0 = Ok

0

9

Reserved

Reserved

0

10

Reserved

Reserved

0

11

Reserved

Reserved

0

12

Reserved

Reserved

0

13

Reserved

Reserved

0

14

Reserved

Reserved

0

15

Reserved

Reserved

0

Notes: --